Module Calibrations

Instrument:
N1000A
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Use the Module tab of the Calibrations dialog to perform the vertical, clock recovery, and precision timebase calibrations on modules installed in a DCA-X's module bay as well as DCA-M modules. Module calibrations enhance measurement precision by establishing calibration factors which compensate for imperfections in the measurement system, such as variations due to the ambient temperature. Module calibrations do not require any external equipment setup.

The following picture shows how the vertical calibration commands correlate with FlexDCA's Calibrations dialog.

The tabs shown in the Calibrations dialog depend on the installed module. For example, the tab for the N1055A module, would include a TDR Step Calibration.

Recommended Module Calibration Conditions

A calibration is recommended whenever any of the following conditions are true:

  • A DCA-X or DCA-M power has been cycled
  • A DCA-X module has been removed and then reinserted since the last calibration
  • The temperature change of a DCA-X or DCA-M exceeds 5°C compared to the temperature of the last module calibration ( ΔT > 5°C)
  • Time since the last calibration has exceeded 7 days.

Always remove or disable all inputs to the module.

The vertical calibration uses known signal levels in the DCA-X. Introducing an outside signal source will interfere with the calibration factors and decrease the accuracy of the calibration.

Re-seating the module into the DCA-X may affect the electrical connections, which in turn affects the data sampling process.

To perform a module calibration

  1. Select which vertical, precision timebase, clock recovery, and TDR calibrations that you want to perform using these commands. When in doubt, you can always use the SCPI Recorder.
  2. Start all selected calibrations with the :CALibrate:SLOT:STARt command.

To query the status of these calibrations, use the following commands: