:CALibrate:SLOT:PTIMebase:STATus:DETails?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B-PTB
Query Syntax
:CALibrate:SLOT{1:8}:PTIMebase:STATus:DETails?
Where the required specifier {1:8} identifies an N1093A/B DCA-M module by slot number.
Description
Queries a string of status details of an N1093A/B DCA-M module's precision timebase calibration for the indicated slot. The following is an example of a typical returned string:
Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
If a calibration is recommended, the following shows an example of the string:
"Elapsed cal time has exceeded 10 hours.,Time of last Calibration: 10/08/2012 11:13:37,Elapsed Calibration Time: 9 days,Temperature Change: -4.32 C"
If a calibration has not yet been performed, the following string is returned:
"This calibration has never been performed in this instrument."
Example Returned Status String
"Requires Clock Recovery Calibration,Time of last Calibration: 03/14/2012 11:52:00,Elapsed Calibration Time: 75 hours 2 minutes,Temperature Change: 3.40 C"
Requires FlexDCA revision A.07.90 and above.
Example Returned Status String
"Precision Timebase Calibration has not been performed since the last Vertical Calibration,Requires Precision Timebase Calibration,Time of last Calibration: 03/01/2012 12:04:00,Elapsed Calibration Time: 56 hours 49 minutes,Temperature Change: 6.20 C"
Example Command
:CALibrate:SLOT3:PTIMebase:STATus:DETails?