:CALibrate:SLOT:PTIMebase
Command Syntax
:CALibrate:SLOT{1:8}:PTIMebase {ENABled | DISabled}
Where the required specifier {1:8} identifies an N1093A/B DCA-M module by slot number.
Query Syntax
:CALibrate:SLOT{1:8}:PTIMebase?
Query Response
{ENAB | DIS}
Description
For the indicated slot, enables or disables the precision timebase calibration for an N1093A/B DCA-M module. To perform this calibration along with all other selected calibrations for the indicated slot, use the :CALibrate:SLOT:STARt command. To select a vertical or clock recovery calibration, use the CALibrate:SLOT:VERTical and CALibrate:SLOT:CRECovery commands. To select all calibrations for the indicated slot, use the CALibrate:SLOT:ENABled command. These commands affect the Calibration dialog indicators, as shown in the following picture.
- ENABled
-
Selects the calibration. - DISabled
-
Prevents the calibration.
Requires FlexDCA revision A.07.90 and above.
Use the child queries listed in the following table to return details about the current calibration.
Example Command
:CALibrate:SLOT3:PTIMebase