:CALibrate:SLOT:PTIMebase:STATus:TIME?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B-PTB
Query Syntax
:CALibrate:SLOT{1:8}:PTIMebase:STATus:TIME?
Where the required specifier {1:8} identifies an N1093A/B DCA-M module by slot number.
Description
Queries the date and time of an N1093A/B DCA-M module's last precision timebase calibration for the indicated slot. If a calibration has not yet been performed, an empty string is returned.
Requires FlexDCA revision A.07.90 and above.
Example Returned Status String
"10/08/2012 11:13:37"
Example Command
:CALibrate:SLOT3:PTIMebase:STATus:TIME?