:CALibrate:SLOT:PTIMebase:STATus?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B-PTB
Query Syntax
:CALibrate:SLOT{1:8}:PTIMebase:STATus?
Where the required specifier {1:8} identifies an N1093A/B DCA-M module by slot number.
Description
Queries the calibration status of an N1093A/B DCA-M module's precision timebase calibration in the indicated slot. One of the following response strings is returned:
- "CALIBRATED"
- The calibration is valid.
- "UNCALIBRATED"
- The calibration is needed.
- ""
- An empty string is returned if the hardware for the indicated slot does not exist. An -241,"Hardware missing" error is returned by the
:SYStem:ERRor:Nextcommand.
Use the child queries listed in the following table to return details about the current calibration.
| Status String | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:DETails?
|
| Change in temperature | :DTEMperature?
|
| Change in Time | :TIME?
|
Requires FlexDCA revision A.07.90 and above.
Example Command
:CALibrate:SLOT3:PTIMebase:STATus?