:CALibrate:SLOT:PTIMebase:STATus:DTEMperature?
Flex Apps:
FlexDCA
FlexRT
Instruments:
N1093A/B-PTB
Query Syntax
:CALibrate:SLOT{1:8}:PTIMebase:STATus:DTEMperature?
Where the required specifier {1:8} identifies an N1093A/B DCA-M module by slot number.
Description
Queries the change in N1093A/B DCA-M module's temperature from the time when the precision timebase calibration was performed on the indicated slot. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in temperature exceeds ±5°C. Use the :CALibrate:SLOT:PTIMebase command to enable a precision timebase calibration.
Requires FlexDCA revision A.07.90 and above.
Example Returned Status
3.590000000E+00
Example Command
:CALibrate:SLOT3:PTIMebase:STATus:DTEMperature?