:CALibrate:SLOT:STEP:STATus:DTEMperature?
Flex Apps:
FlexDCA
Meas. mode:
TDR
Query Syntax
:CALibrate:SLOT{1:8}:STEP:STATus:DTEMperature?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
Returns a string that provides the change in temperature (Celsius) from the last TDR module's step calibration. Use the :CALibrate:SLOT:STEP:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string, which indicates that the temperature of the N1000A has risen 1.73°C:
"1.730000000E+00"
Requires FlexDCA revision A.04.00 and above.
Example Command
:CALibrate:SLOT3:STEP:STATus:DTEMperature?