:CALibrate:SLOT:STEP:STATus:TIME
Flex Apps:
                                                FlexDCA
                                            Meas. mode:
                                                TDR
                                            Query Syntax
:CALibrate:SLOT{1:8}:STEP:STATus:TIME?
                                            Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
Returns a string that provides the time that has elapsed since the last TDR module's step calibration. Use the :CALibrate:SLOT:STEP:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"01/09/2014 06:20:09"
Requires FlexDCA revision A.04.00 and above.
Example Command
:CALibrate:SLOT3:STEP:STATus:TIME?