:CALibrate:SLOT:STEP:STATus:DETails?
Flex Apps:
FlexDCA
Meas. mode:
TDR
Query Syntax
:CALibrate:SLOT{1:8}:STEP:STATus:DETails?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
Returns a string that provides the date of the last TDR module's step calibration as well as the elapsed time and the temperature (Celsius) change. Use the :CALibrate:SLOT:STEP:STATus? parent query to determine if a calibration is needed and how the calibration is made.
The following is an example of the returned string:
"Time of last Calibration: 01/08/2014 07:07:12,Elapsed Calibration Time: 8 days,Temperature Change: 1.73 C"
Requires FlexDCA revision A.04.00 and above.
Example Command
:CALibrate:SLOT3:STEP:STATus:DETails?