:CALibrate:SLOT:STEP:STATus?
Flex Apps:
FlexDCA
Meas. mode:
TDR
Query Syntax
:CALibrate:SLOT{1:8}:STEP:STATus?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Query Response
{CALIBRATED | UNCALIBRATED}
Description
Returns the status of the TDR step calibration for N1055A or 54754A TDR/Electrical modules. Use the :DETails, :DTEMperature, and :TIME child commands to return detailed information about the calibration status. Use the :CALibrate:SLOT:STEP command to enable the step calibration.
Requires FlexDCA revision A.04.00 and above.
Example Command
:CALibrate:SLOT3:STEP:STATus?