:CHANnel:BANDwidth
Command Syntax
:CHANnel{1:8}{A|B|C|D}:BANDwidth {BANDwidth{1:16}}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:BANDwidth?
Description
Selects the sampler bandwidth (in Hz) of an electrical or optical channel. There can be up to 16 supported sampler bandwidth settings, depending on the module. The sampler bandwidth affects the width of the sampling pulse used by the instrument. Wider bandwidths allow the instrument to respond to fast changes in a waveform. The increased bandwidth yields the highest measurement fidelity. Narrow bandwidth offers the best sensitivity by reducing the noise on the input waveform while still maintaining good frequency response. A lower sampler bandwidth is especially useful for low-level signals that cannot be averaged.
The command argument identifies a bandwidth setting that is:
- For electrical channels, shown in the Bandwidth field of the Channel Setup dialog. For example,
BANDwidth2identifies the second from the top listing, 15.0 GHz, shown in this picture. - For optical channels, shown in the Sampler Bandwidth field of the Advanced settings in the Channel Setup dialog. For example,
BANDwidth2identifies the second from the top listing, 15.0 GHz, shown in this picture.
Recommended Alternative
The following commands are the preferred method of setting the channel bandwidth as they set the value explicitly rather than implicitly thereby making your code more reliable and easier to read:
- To set bandwidth, use
:CHANnel:BANDwidth:FREQuency - To select maximum bandwidth, use
:CHANnel:BANDwidth:FREQuency:MAXimum - To select minimum bandwidth, use
:CHANnel:BANDwidth:FREQuency:MINimum - To return a list of available sampler bandwidths, use the
:CHANnel:BANDwidth:FREQuency:VSET?
Example Command
The following command selects the second sampler bandwidth selection shown in the Channel Setup dialog.
:CHANnel2A:BANDwidth BANDwidth2
or
:CHANnel2A:BANDwidth:FREQuency 15.0E9