:CHANnel:BANDwidth:FREQuency:MINimum
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CHANnel{1:8}{A|B|C|D}:BANDwidth:FREQuency:MINimum
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:BANDwidth:FREQuency:MINimum?
Description
If the sampler bandwidth for the module can be changed, sets the bandwidth to its minimum supported value.
- To set the bandwidth to its maximum value, use the
:CHANnel:BANDwidth:MAXimumcommand. - To set or query the current bandwidth, use the
:CHANnel:BANDwidth:FREQuencycommand.
Requires FlexDCA revision A.05.30 and above.
Example Command
:CHANnel2A:BANDwidth:FREQuency:MINimum