:CHANnel:BANDwidth:FREQuency:VSET?
Query Syntax
:CHANnel{1:8}{A|B|C|D}:BANDwidth:FREQuency:VSET?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries a list of available sampler bandwidths in Hz for the selected channel. For example,
"12.40E+9,20.00E+9,…"
The bandwidths in the returned list are in the same order as they are listed in the Bandwidth field of the Channel Setup dialog (electrical channels) or the Sampler Bandwidth field of the Advanced settings in the Channel Setup dialog (optical channels). To select a bandwidth based on its position in the dialog list, use the :CHANnel:BANDwidth command. To select a bandwidth based on its frequency, use the :CHANnel:BANDwidth:FREQuency command.
Requires FlexDCA revision A.05.30 and above.
Example Command
:CHANnel2A:BANDwidth:FREQuency:VSET?