:CHANnel:RTSCope:INTerpolate:FACTor
Command Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:INTerpolate:FACTor <factor>
Where <factor> is an integer.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:INTerpolate:FACTor?
Description
For the selected channel, specifies a factor (integer value) that determines the number of points FlexRT uses to interpolate between points on the real-time oscilloscope's waveform. To select the interpolation method, use the :CHANnel:RTScope:INTerpolate:METHod command. The number of sample-per-UI in the interpolated waveform is:
(acquired samples-per-UI) (factor) = samples-per-UI
You can also directly set the sample-per-UI using the :CHANnel:RTScope:INTerpolate:SPUI command.
Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:RTSCope:INTerpolate:FACTor 2