:CHANnel:RTSCope:SRATe:AUTodetect
Command Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:SRATe:AUTodetect {ON | OFF | 1 | 0}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:SRATe:AUTodetect?
Query Response
{1 | 0}
Description
For the selected channel, enables or disables automatic symbol-rate detection. When turned off, use the :CHANnel:RTSCope:SRATe command to set the symbol rate.
Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:RTSCope:SRATe:AUTodetect ON