:CHANnel:RTSCope:SRATe
Command Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:SRATe <rate>
<rate> is a double.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:SRATe?
Description
For the selected channel, enters the symbol-rate of input channel waveform from the UXR-series oscilloscope. Automatic detection must be turned off before the entered symbol-rate setting is applied (:CHANnel:RTSCope:SRATe:AUTodetect).
Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:RTSCope:SRATe 9.9532800E+09