:CHANnel:UDEFined:PROXimal
Command Syntax
:CHANnel{1:8}{A|B|C|D}:UDEFined:PROXimal <amplitude>
<amplitude> is a double.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:UDEFined:PROXimal?
Description
Sets or queries the lower threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:PROXimal command.
Use the :MEASure:THReshold:METHod command to specify the use of custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels base on absolute amplitude values.
Use the :CHANnel{N}:UDEFined:DISTal command to enter a upper threshold level. Use the :CHANnel{N}:EMEMory:MESial command to enter a middle threshold level.
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs UNITs :MEASure:UTSRc CHANnel1 :CHANnel2a:UDEFined:DISTal 125E-3 :CHANnel2a:UDEFined:MESial 0E0 :CHANnel2a:UDEFined:PROXimal -125E-3