:MEASure:THReshold:PROXimal
Command Syntax
:MEASure:THReshold:PROXimal <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:THReshold:PROXimal?
Description
Sets or queries the lower threshold-definition level. This value is used when making duty cyle distortion, rise time, and fall time measurements with custom threshold definitions based on percent. When custom threshold definitions are based on absolute amplitude, use the :CHANnel, :EMEMory, :FUNCtion, or :WMEMory command refered to in :MEASure:THReshold:METHod.
Use the :MEASure:THReshold:METHod command to use custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels base on percentages.
Use the :MEASure:THReshold:DISTal command to enter a upper threshold level. Use the :MEASure:THReshold:MESial command to enter a lower threshold level.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
| Threshold | Approximate Limits | ||
|---|---|---|---|
| % | Units | ||
| Volts (electrical) |
Watts (optical) |
||
| Maximum* | 125% | 429 mV | 676 μW |
| Default* | 10% | 0V | 200 μW |
| Minimum | –25% | –429 mV | –175 μW |
| *. Limited by middle threshold's setting. | |||
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs PERCent :MEASure:THReshold:DISTal 9.50E+1 :MEASure:THReshold:MESial 5.0E+1 :MEASure:THReshold:PROXimal 1.50E+1