:CRECovery:JSANalysis:PLLoop:MODE
Instrument:
N1000A
N107x
N1060A
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4
Command Syntax
:CRECovery{1:8}:JSANalysis:PLLoop:MODE {JTF | OJTF}
Where the {1:8} specifier identifies a slot number. The slot number is associated with the N1060A, N1076A/B, N1077A, N1078A, or 86108B module with Option JSA. When an 86108B module is used, the slot number is always 1.
Query Syntax
:CRECovery{1:8}:JSANalysis:PLLoop:MODE?
Query Response
{JTF | OJTF}
Description
Defines either the Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF) for first- or second-order PLL loops. To select the loop order, use the :CRECovery1:JSANalysis:PLLoop:ORDER command.
- JTF
- Specify the loop bandwidth with the
:CRECovery1:JSANalysis:PLLoop:JTF:BWIDthcommand. For second-order loops, define the loop peaking using the:CRECovery1:JSANalysis:PLLoop:JTF:PEAKingcommand. - OJTF
- Specify the loop bandwidth with the
:CRECovery1:JSANalysis:PLLoop:OJTF:BWIDthcommand. For second-order loops, define the loop damping factor using the:CRECovery1:JSANalysis:PLLoop:JTF:DFACtorcommand.
Requires FlexDCA revision A.01.70 and above.
Requires a clock-recovery module that has Option JSA (Jitter Spectrum Analysis and SW Clock Recovery Emulation).
Command Compatibility
- N1060A Option JSA
- 86108A/B Option JSA
- N107X-series Option JSA
Example Command Sequence
:CRECovery{1:8}:JSANalysis:PLLoop:MODE JFT