:DISPlay:JITTer:SGRaph:STARt
Meas. mode:
Jitter
Package License:
L-RND
Flex Apps:
FlexDCA
Command Syntax
:DISPlay:JITTer:SGRaph:STARt <start_symbol>
<start_symbol> is an integer.
Query Syntax
:DISPlay:JITTer:SGRaph:STARt?
Description
Sets the starting symbol displayed in the DDJ versus Symbol and ISI versus Symbol graphs (:DISPlay:JITTer:GRAPh:TYPE). Use :DISPlay:JITTer:SGRaph:RANGe to set the number of symbols displayed in the graphs. Use the :MEASure:JITTer:DDJSymbol? query to return the data.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :DISPlay:JITTer:DDJVsbit:START.