:DISPlay:WINDow:MAGNitude:LEGend:EXPand
Command Syntax
:DISPlay:WINDow:MAGNitude{N}:LEGend:EXPand {ON | OFF}
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:MAGNitude{N}:LEGend:EXPand?
Description
Expands or contracts the Signals legend that is shown in the Freq-Mag waveform content window. The legend shows TDR Mode S-parameters. The legend also shows any output waveforms of the FFT function (FFT command) (when defined as magnitude). To completely remove the signal legend from all frequency-domain windows, use the :WINdow:FDLegend command.
Requires FlexDCA revision A.03.00 and above.