:DISPlay:WINDow:T:OHMS:TWDouble
TDR
Command Syntax
:DISPlay:WINDow:T:OHMSN:TWDouble {ON | OFF | 1 | 0}
Where N indicates one of 4 possible GrpDelay windows. For example, :T:OHMS2.
Query Syntax
:DISPlay:WINDow:T:OHMSN:TWDouble?
Query Response
{1 | 0}
Description
When the Time-Ohm waveform content window is displayed, use this command to specify the width of the Time-Ohm waveform content window. The window can full width (ON) or half width (OFF). Use the :DISPlay:WINDow:T:OHMS:LOCation command to align the window with either the left or right edge of the waveform window.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:T:OHMS2:TWDouble OFF :DISPlay:WINDow:T:OHMS2:LOCation RSECondary :DISPlay:TSMode HSIZe