:DISPlay:WINDow:T:PERCent{N}:ZSIGnal
Command Syntax
:DISPlay:WINDow:T:PERCent{N}:ZSIGnal TRACe{1:128}
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:T:PERCent{N}:ZSIGnal?
Description
When a Time-% waveform content window is displayed in zoom tiled mode and there are multiple displayed waveforms, selects a waveform to display in the graticule area. TDR Mode's time-domain parameters can be viewed in a Time-% window.
Requires FlexDCA revision A.04.00 and above.