:DISPlay:WINDow:TIME:ZSIGnal
Command Syntax
:DISPlay:WINDow:TIME{1}:ZSIGnal
Query Syntax
:DISPlay:WINDow:TIME{1}:ZSIGnal?
Description
When a Waveform content window is displayed in zoom tiled mode and there are multiple displayed waveforms, selects a waveform to display in the graticule area. Channel and differential channel waveforms can be viewed in a Waveform content window.
Requires FlexDCA revision A.03.00 and above.