:EMEMory:FILE:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:FILE:LOAD
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Loads the selected waveform file into the indicated eye-memory location. Use the :EMEMory:FILE:NAME command to specify the name of the file to load. Use the :EMEMory:DISPLay command to display the eye-memory waveform.
To load a waveform source into memory, for example channel 1A, use the :EMEMory:LOAD command.
Requires FlexDCA revision A.05.70 and above.
Example Command
:EMEMory3:FILE:LOAD