:EMEMory:FILE:NAME
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:FILE:NAME "filename"
Where the required specifier {1:8} identifies one of eight eye memories.
Where "filename" is the imported file.
Query Syntax
:EMEMory{1:8}:FILE:NAME?
Query Response
"string"
Description
Enters the name (including path) of a file to be imported into an eye memory using the :EMEMory:FILE:LOAD command. If no path is given, the file expected to be in the default \Colorgrade-Grayscale folder.
Requires FlexDCA revision A.05.70 and above.
Example Command
:EMEMory3:FILE:NAME "CGMemory2.cgsx"