:EMEMory:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:LOAD
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Loads the selected waveform source into the indicated eye-memory location. Use the :EMEMory:LOAD:SOURce command to select the source. Use the :EMEMory:DISPLay command to display the eye-memory waveform.
To load a color grade-gray scale file into eye memory, use the :EMEMory:FILE:LOAD and :EMEMory:FILE:NAME commands.
Example Command Sequence
:EMEMory2:LOAD:SOURce CHAN1A :EMEMory2:LOAD :EMEMory2:DISPLay ON