:EMEMory:LOAD:SOURce
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:LOAD:SOURce <source_waveform>
Where the required specifier {1:8} identifies one of eight eye memories.
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:EMEMory{1:8}:LOAD:SOURce?
Description
Selects the source waveform to load into eye memory. Use the :EMEMory{1:8}LOAD command to actually load the selected source.
Example Command Sequence
:EMEMory2:LOAD:SOURce CHAN1A :EMEMory2:LOAD