:FRAMe:SWITch:VERify:CONTinue
Instruments:
N1002A
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG
Command Syntax
:FRAMe:SWITch:VERify:CONTinue
Description
Continues the switch port verification pass/fail test. As a test progresses, message or decision dialogs often appear. For example, the user might be instructed to connect a fiber optic cable to a different port on the switch. This command is equivalent to clicking the dialog's Next or Done button. Use the :FRAMe:SWITch:VERify:CANCel command for an equivalent of the Cancel button.
Follow this command with the query to control program timing.:FRAMe:SWITch:VERify:SDONe?
This command requires FlexDCA revision A.07.40 and above.