:FRAMe:SWITch:ROUTe:LIST?
Instruments:
N1002A
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG
This command only applies to demo and evaluation N1002A-S40 instruments.
Query Syntax
:FRAMe:SWITch:ROUTe:LIST? ["<switch-ID>"]
Where <switch-ID> is an optional parameter that identifies an internal switch on N1002A switch.
Query Response
"1.1,1.2,1.3,1.4,1.9,1.10,1.11,1.12,2.1,2.2,2.3,2.4,2.9,2.10,2.11,2.12,3.1,3.2,3.3,3.4,3.9,3.10,3.11,3.12,4.1,4.2,4.3,4.4,4.9,4.10,4.11,4.12,6.1,6.2,6.3,6.4,6.9,6.10,6.11,6.12"
Description
Returns a comma separated string of all optical switch ports.
This command requires FlexDCA revision A.07.40 and above.