:FRAMe:SWITch:ROUTe:VSET?
Instruments:
N1002A
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG
This command only applies to demo and evaluation N1002A-S40 instruments.
Query Syntax
:FRAMe:SWITch:ROUTe:VSET? "<switch-port>"
Where <switch-port> identifies any port on the N1002A-S40 optical switch.
Query Response
For switch port "1.1" returns "DISCONNECTED,6.1,6.2,6.3,6.4,6.9,6.10,6.11,6.12".
Description
For a specified <switch-port>, returns the set of all switch ports ID string arguments (including "DISCONNECTED") that you can send as a destination argument to the :FRAMe:SWITch:ROUTe command. For the example query response shown above, you could select port "6.4" as in:
:FRAMe:SWITch:ROUTe "1.1", "6.4"
This command requires FlexDCA revision A.07.40 and above.