:FRAMe:SWITch:VERify:CHANnel
Instruments:
N1002A
Flex Apps:
FlexDCA
Package License:
L-RND
L-MFG
This command only applies to demo and evaluation N1002A-S40 instruments.
Command Syntax
:FRAMe:SWITch:VERify:CHANnel
Query Syntax
:FRAMe:SWITch:VERify:CHANnel?
Description
Specifies the receiver module (DCA-X or DCA-M) input channel that is used to measure the signal on the switch's output.
This command requires FlexDCA revision A.07.40 and above.