:FUNCtion:UDEFined:DISTal
Command Syntax
:FUNCtion{1:64}:UDEFined:DISTal <amplitude>
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Where <amplitude> is an double.
Query Syntax
:FUNCtion{1:64}:UDEFined:DISTal?
Description
Sets or queries the upper threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:DISTal command.
Use the :MEASure:THReshold:METHod command to specify the use of custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels base on absolute amplitude values.
Use the :FUNCtion{1:16}:UDEFined:MESial command to enter a middle threshold level. Use the :FUNCtion{1:16}:UDEFined:PROXimal command to enter a lower threshold level.
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs UNITs :MEASure:UTSRc CHANnel1 :FUNCtion3:UDEFined:DISTal 125E-3 :FUNCtion3:UDEFined:MESial 0E0 :FUNCtion3:UDEFined:PROXimal -125E-3