:MEASure:THReshold:DISTal
Command Syntax
:MEASure:THReshold:DISTal <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:THReshold:DISTal?
Description
Sets or queries the upper threshold-definition level. This value is used when making certain measurements with custom threshold definitions based on percent. When custom threshold definitions are based on absolute amplitude, use the :CHANnel, :EMEMory, :FUNCtion, or :WMEMory command refered to in :MEASure:THReshold:METHod. This command is equivalent to the settings in the Thresholds tab of the Configure Measurements dialog.
Use the :MEASure:THReshold:METHod command to use custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels based on voltage or percentages.
Use the :MEASure:THReshold:MESial command to enter a middle threshold level. Use the :MEASure:THReshold:PROXimal command to enter a lower threshold level.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
| Threshold | Approximate Limits | ||
|---|---|---|---|
| % | Units | ||
| Volts (electrical) |
Watts (optical) |
||
| Maximum | 125% | 429 mV | 676 μW |
| Default* | 90% | 0V | 200 μW |
| Minimum* | –25% | –429 mV | –175 μW |
| *. Limited by middle threshold's setting. | |||
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs PERCent :MEASure:THReshold:DISTal 9.50E+1 :MEASure:THReshold:MESial 5.0E+1 :MEASure:THReshold:PROXimal 1.50E+1