:GRAPh:T:VOLTs:X:UNITs

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA

Command Syntax

:GRAPh:T:VOLTs{1:4}:X:UNITs {SECond | METer}

Where the {1:4} specifier identifies one of four waveform content windows.

Query Syntax

:GRAPh:T:VOLTs{1:4}:X:UNITs?

Description

For the specified Time-Volts waveform content window, sets the X-axis units to be either time (seconds) or distance (meters). When meters are selected, you can accurately scale the X-axis distance for the velocity of propagation through the DUT path. This can be accomplished by entering either the DUT's Velocity Factor (:VFACtor sibling command) or Dielectric Constant (εr) (:DCONstant sibling command). Defining the X-axis in meters allows you to directly measure the cable and trace lengths or correlate the impedance of discontinuities with physical structures such as connectors and vias.

If you save a Time-Volts waveform to a file, the file's X-axis units will be the same as the displayed graph. When the file is recalled into a waveform memory, it can only be displayed in a Time-Volts graph that has the same X-axis units as defined in the file. The default setting is time (seconds).

TDR/TDT mode's T-parameter responses are the source of Time-Volts waveforms.

Requires FlexDCA revision A.04.20 and above.