:GRAPh:T:VOLTs:Y:OFFSet
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:GRAPh:T:VOLTs{1:4}:Y:OFFSet <volts>
Where the <volts> is a double.
Where the {1:4} specifier identifies one of four waveform content windows.
Query Syntax
:GRAPh:T:VOLTs{1:4}:Y:OFFSet?
Description
Sets the vertical offset of the specified Time-Volts content window in volts at the Y-axis's center graticule. Use the :AUToscale sibling command to automatically set the offset and scale settings. Use the :AUToscale parent command to automatically scale both the waveform in both X and Y axis.
Requires FlexDCA revision A.04.00 and above.