:JSAMemory:FILE:NAME
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:FILE:NAME "filename"
Query Syntax
:JSAMemory:FILE:NAME?
Query Response
"filename"
Description
Enters the name (including path) of a file to be imported into an jitter spectrum analysis memory using the :JSAMemory:FILE:LOAD command. If no path is given, the file expected to be in the default \Jitter Data folder.
Requires FlexDCA revision A.05.70 and above.