:JSAMemory:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:LOAD
Description
Loads the current jitter spectrum analysis data into jitter memory. Use the :JSAMemory:LOAD:SOURce command to select the source, for example channel 1A. Use the :JSMemory:DISPLay command to display graphs and scalar data from the jitter memory.
To load a jitter spectrum analysis file into jitter spectrum analysis memory, use the :JSAMemory:FILE:LOAD and :JSAMemory:FILE:NAME commands.
To save JSA data to a file, use the :DISK:JSANalysis:SAVE command.
Requires FlexDCA revision A.05.70 and above.
Child Commands
:SOURcespecifies the source waveform on which to perform the measurement.