:JSAMemory:FILE:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:FILE:LOAD
Description
Loads the selected jitter spectrum analysis data file into jitter spectrum analysis memory. Use the :JSAMemory:FILE:NAME command to specify the name of the file to load. Use the :JSAMemory:DISPLay command to display the jitter-memory waveform.
To load JSA data for a waveform source into memory, for example channel 1A, use the :JSAMemory:LOAD command.
Requires FlexDCA revision A.05.70 and above.