:JSAMemory:LOAD:SOURce
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:LOAD:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:JSAMemory:LOAD:SOURce?
Query Response
<source_waveform>
Description
Specifies the source waveform for the currently jitter spectrum analysis data that will be loaded into jitter spectrum analysis memory using the command.:JSAMemory:LOAD
Requires FlexDCA revision A.05.70 and above.