:LTESt:ACQuire:SIMage:FNAMe:AUPDate
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:ACQuire:SIMage:FNAMe:AUPDate
Description
Increments a file name's autonumber for the next screen-capture reporting file for an acquisition limit test. Use the :LTESt:ACQuire:SIMage:STATe command to enable and disable screen-capture reporting. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command. The autonumber format is explained in :LTESt:ACQuire:SIMage:FNAMe.
Requires FlexDCA revision A.05.70 and above.
Example Command Sequence
:ACQuire:SINGle :LTESt:ACQuire:SIMage:FTYPe PNG :LTESt:ACQuire:SIMage:FNAMe "my_file_1" :LTESt:ACQuire:SIMage:STATe ON // Enable screen capture reporting :LTESt:ACQuire:STATe ON // Turn limit test on :ACQuire:RUN;*OPC? # my_file_1.png … … :ACQuire:CDISplay :LTESt:ACQuire:SIMage:FNAMe:AUPDate :ACQuire:RUN;*OPC? # my_file_2.png