:LTESt:ACQuire:SIMage:MONochrome
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:ACQuire:SIMage:MONochrome {ON | OFF | 1 | 0}
Query Syntax
:LTESt:ACQuire:SIMage:MONochrome?
Query Response
{1 | 0}
Description
Turns monochrome screen capture on and off when reporting a screen capture for an acquisition limit test. When on, a black and white image will be captured and saved into a file by the :LTESt:ACQuire:SIMage:FNAMe command. Selecting monochrome automatically inverts the graticule area's background color. Use the :LTESt:ACQuire:SIMage:STATe command to enable screen captures to be saved when the limit test completes. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.
Example Command
:LTESt:ACQuire:SIMage:MONochrome ON