:LTESt:ACQuire:SIMage:WINDow
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:ACQuire:SIMage:WINDow {DISPlay | TIMe{1} | GDELay{1:4} | MAGNitude{1:4} | PHASe{1:4}}
Query Syntax
:LTESt:ACQuire:SIMage:WINDow?
Query Response
{1 | 0}
Description
When reporting a screen image as a result of an acquisition limit test, use this command to selects which portion of the screen to include in the image. To actually specify that a screen image is saved, use the :LTESt:ACQuire:SIMage:STATe command. The following selections are available:
- DISPlay
- Includes the entire FlexDCA screen in the captured screen image.
- TIMe1
- Includes only the Waveform content window in the captured screen image.
- GDELay{1:4}
- Includes only the Delay 1, Delay 2, Delay 3, or Delay 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Delay windows 2, 3, and 4 can only be displayed programatically and not using front-panel controls. The group Delay window can be selected as a display output format for FFT functions (
:FUNCtion:FOPerator FFT). - MAGNitude{1:4}
- Includes only the Magnitude 1, Magnitude 2, Magnitude 3, or Magnitude 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Magnitude windows 2, 3, and 4 can only be displayed programatically and not using front-panel controls. The group Magnitude window can be selected as a display output format for FFT functions (
:FUNCtion:FOPerator FFT). - PHASe{1:4}
- Includes only the Phase 1, Phase 2, Phase 3, or Phase 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Phase windows 2, 3, and 4 can only be displayed programatically and not using front-panel controls. The group Phase window can be selected as a display output format for FFT functions (
:FUNCtion:FOPerator FFT).
Requires FlexDCA revision A.03.00 and above.
Example Command
:LTESt:ACQuire:SIMage:WINDow DISPlay