:ACQuire:STOP
Instrument:
N1010A
N1000A
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:ACQuire:STOP
Description
Stops data acquisition. This command is equivalent to clicking the Stop button. This command does not erase display memory. To clear display memory, use the :ACQuire:CDISplay command. Use the :ACQuire:RUN command to resume data acquisition. When acquisition is stopped, use the :ACQuire:SINGle command to start a single run of capturing waveform data.