:MEASure:EYE:PAM:ELEVel

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:ELEVel

Query Syntax

:MEASure:EYE:PAM:ELEVel?

Description

Starts Eye/Mask mode's Eye PAM4/6/8 Level measurement where the center amplitude of the selected eye (vertical center) of a PAM signal is measured. Select the eye to be measured using the :MEASure:EYE:PAM:ELEVel:EYE child command. To measure the eye levels for all of the eyes on a PAM4 signal, you must send this command once for each eye as there is no command for simultaneously measuring all eye levels. The query form of the command returns the measured value. Sources can be any displayed PAM or NRZ waveform from a channel, differential channel, color-grade memory, or function. For example, CHAN1A, CGMemory1, or FUNCtion1.

Related Commands

Command Equivalent Setting
in PAM-N Analysis Setup Dialog
Description
:MEASure:PAM:EYE:ESTiming Receiver Sample Timing Configures the timing for sampling the signal data for all PAM measurements in Eye/Mask mode.
:MEASure:PAM:EYE:ELMethod Eye Center Location Selects the basis for determining the location of an eye's center on the waveform: at maximum eye width or maximum eye height.
:MEASure:PAM:EYE:PPERcent Eye Level Width Defines the timespan (in percentage of symbol width) over which an eye's amplitude level is measured.
:MEASure:PAM:AMPLitude:UNITs Amplitude Units Sets the amplitude units for measurement: volts, Watts, or percent.

Measurement Identification

Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.

For example, to return the status of the measurement, :MEASure:EYE:PAM:ELEVel

flex.write(':MEASure:EYE:PAM:ELEVel:SOURce CHAN1A')
if flex.query(':MEASure:EYE:PAM:ELEVel:STATus?') == 'CORR';
    measurement = flex.query(':MEASure:EYE:PAM:ELEVel?')
else:
	details = flex.query(':MEASure:EYE:PAM:ELEVel:STATus:DETails?')
	reason = flex.query(':MEASure:EYE:PAM:ELEVel:STATus:REASon?')

Child commands for measurement identification:

  • :MEASure:EYE:PAM:ELEVel:SOURce

This Eye mode measurement can be applied to both NRZ and PAM4 waveforms.

Requires FlexDCA revision A.04.50 and above.

Example Command Sequence

:MEASure:EYE:PAM:ELEVel:SOURce CHAN1A
:MEASure:PAM:AMPLitude:UNITs PERCent
:MEASure:EYE:PAM:ELEVel:EYE EYE2
:MEASure:EYE:PAM:ELEVel
:MEASure:EYE:PAM:ELEVel?