:MEASure:PAM:EYE:ESTiming
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:EYE:ESTiming {CEYE | PELevel}
Query Syntax
:MEASure:PAM:EYE:ESTiming?
Description
Configures the timing for sampling the signal data for all PAM measurements in Eye/Mask mode. Use this setting to match the timing method used by a receiver. For signals with skewed eyes, measurements results will vary depending on this setting. This setting does not apply to PAM4 measurements in Oscilloscope mode.
| Arguments | Description |
|---|---|
| CEYE | Sampling timing is based on the location of the center eye (labeled Eye 1/2 in the following picture). This is the default setting. |
| PELevel | Sampling timing is independently based on the location of each of the three eyes. |
Requires FlexDCA revision A.04.50 and above.