:MEASure:PAM:EYE:ELMethod
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:EYE:ELMethod {MEWidth | MEHeight}
Description
Selects the basis for determining the location of an eye's center on the waveform. This setting affects all PAM4 measurements in Eye mode. It does not affect PAM4 measurements in Oscilloscope mode.
| Arguments | Description |
|---|---|
| MEWidth | The eye's center is located at the eye's maximum width midway between the eye's inside left and right edges. This is the default setting. |
| MEHeight | The eye's center is located at the eye's maximum height midway between the eye's inside top and bottom edges. |
Requires FlexDCA revision A.04.50 and above.