:MEASure:PAM:EYE:PPERcent
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:EYE:PPERcent <% value>
<% value> is a double.
Query Syntax
:MEASure:PAM:EYE:PPERcent?
Description
Defines the timespan over which an eye's amplitude level is measured. The timespan is specified as a percentage of the symbol period. The default setting is 10%. This setting affects all PAM4 measurements in Eye mode except Eye Widths (EYE:PAM:EWidth). It does not affect PAM4 measurements in Oscilloscope mode.
Requires FlexDCA revision A.04.50 and above.