:MEASure:EYE:PAM:EWIDth:DEFine:EOPening
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
EYE:PAM:EWIDth:DEFine:EOPening {ZHITs | PROBability}
Query Syntax
EYE:PAM:EWIDth:DEFine:EOPening?
Description
Selects the method used to determine the eye-opening: zero hits (ZHITs) or probability (PROBabilitly). If probability is selected, use the :DEFine:EOPening:PROBability child command to enter the probability. The entered measurement-hit probability establishes the contour of an eye's opening. The default value is 1 x 10–18.
Requires FlexDCA revision A.04.50 and above.