:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSTabilize
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSTabilize {ON | OFF}
Query Syntax
:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSTabilize?
Description
Turns on or off RN stabilization for PAM4 Eye Width and Eye Height measurements. When RN stabilization is on, use the :MEASure:EYE:PAM:EHWIDth:DEFine:EOPening:RNSValue command to enter the RN value. To measure the RN, switch the N1000A to Jitter Mode and measure the RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. The following lists show the linked RNSTabilize and RNSValue commands for EHeight and EWIDth. For example, setting RN stabilization on for EWIDth also turns it on for EHeight.
Linked PAM4 Stabilization (On / Off) Commands
- :MEASure:EYE:PAM:EHeight:DEFine:EOPening:RNSTabilize
- :MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSTabilize
Linked PAM4 Value Commands
Requires FlexDCA revision A.05.30 and above.